Other Parts Discussed in Thread: BQ24650, BQ25895
I have recently ordered the BQ24650EVM-639 module and have been trying to use it for mttp. When connecting a solar panel as Vin and the resistive load as Vsys and a 12V battery as Vout, the voltage is not regulating the input voltage to 17.8 V. The input voltage is approximately 22 V, is more needed to get the voltage to regulate at the input? I went through the test summary, so I know the module is working fine.