Hi,
I have an application where Output from the SMPS(24V) is given to the Controller.In case of Power Outage Controller doesn't have to shut down for 3 sec when Outage occurs.
So I thought of using BQ33100 with this 3.4F 27V Super caps SCAP,PBLS-3.4/27.
I have few question regarding while integrating with the BQ33100.
How do I set the discharge period ?
Are there any reference design example for using BQ33100 with Super Caps?
Thanks.