Dear colleagues,
I am evaluating the BQ28Z610 integrated circuit in order to combine in with two-cell Li-Po or Li-Ion battery. My goal is to have, as stated in datasheet, gas gauge, protection, but also a battery charger.
At this moment I am not 100% sure about its charging ability because I didn't saw that anyone has used it as a charger but only as a gas gauge and protection IC, and in the headline, it is stated that this IC is a gas gauge and a protection solution, without noting the charge feature which is not a small thing.
On the other side in the description, there is a paragraph that says the following:
The Texas Instruments bq28z610 device is a highly integrated, accurate, 1-series to 2-series cell gas gauge and protection solution, enabling autonomous charger control and cell balancing.
I would like to use this IC because it simplifies a development a lot since it integrates all three things in one IC that I need. So, I will be very grateful for your comments and experiences with this IC.
Best regards
Marko