Hi,
I created my POE project with the TPS23756(Part number TPS23756PWPR, digikey partnumber 296-39368-1-ND).
The design is similar as the document SLVU329A <User's Guide TPS23756EVM.pdf> page 4, figure 1. I do not use the adapter, so I removed the adapter block in figure 2. Based on this change, I floated the T2P, tied APD to ARTN through 1K resistor, PPD to VSS through 1K resistor.
The schematic as the inserted .pdf file.
The problem now:
1, The first try with the PCB, I can always get the 50V from power supplier via Ethernet cable, and it's stable --- which indicates the handshaking is correct.
But there is no output behind the main transformer. I checked the VB/CTL, both are 0V, and GATE/GAT2 have no signal output; which are different from the EVM board.
2, I guess maybe the POE chip has broken(the resistor value is about 470 ohms between VB to ARTN), then I replaced it with another one(the resistor value then becomes same as the EVM). With the new TPS23756 chip, the 50V from power supplier via Ethernet cable becomes to unstable --- It will has 50V about a second, then drop to 0V; after a while(3-5 seconds), the 50V comes again, and drop to 0V.
Both VB/CTL have some voltages changing (drop from 0.6V to 0V, maybe due to the unstable of the 50V input). Both GATE/GAT2 has not output(no signal read by the oscilloscope). Maybe due to the on/off of the 50V, I can get 0.5V unstably after the main transformer.
I checked the soldering, it's good. Please help to find the problem, I appreciate your help!
Regards,
Kevin