This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCD90320: check the connection and the R and C value from UCD to VR side

Part Number: UCD90320


I would like to ask UCD.MON and UCD.Margin pin of UCD90320 to connect to the voltage divider resistors of P1V05 and PVTT. The output voltage of these two sets of power supply is the voltage after the voltage divider resistor, which is not the FB pin of VR. want to confirm two things: reference to the attached circuit (a) is there any error in the connection? (b) whether the resistance and capacitance value of the VR terminal connected to the UCD need to be modified (for example, the P1V05 group,UCD question.rar R1063, R1076, C1848 values need to be modified? Please let me know if you need to provide other information, thank you!