This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

WEBENCH® Tools/LM5036: 48V to 12V@170A

Part Number: LM5036
Other Parts Discussed in Thread: UCC28951

Tool/software: WEBENCH® Design Tools

Hi,

I am trying to generate design with 48V in and 12V@170A out requirement

(only current is higher compare to LM56036EVM)

But WEBENCH is giving error.....

All inputs are within limits... then why there is error. 

Is it problem with webench tool or it is invalid  input because of some other parameter?