Other Parts Discussed in Thread: TPSM846C23
Hi,
I would like to extend the remote sensing points in TPSM846C23EVM-806 but I am little bit confused. The block diagram below is what I want to test exactly to see it TPSM846C23 regulates the output properly. I added a diode into the circuit so that I can adjust the voltage across the load starting from 0V. Hoping that TPSM846C23 will adjust its output until the voltage is equal to the commanded votlage (VDC_COMMMAND).
Here is what user guide suggest if remote sensing pins are needed to be extended to another sense point as in my case.
"The EVM uses remote sense connections to regulate the output voltage at the output terminals of the EVM. The remote sense connections are made through 0 O resistors, R16 and R18. If remote sense is required at a different point, R16 and R18 can be replaced with 10 O resistors and VS+ and VS- test points can be extented to the new sense point."
I am a bit confused how to do this properly. I can easily replace the R16 and R18 but I can not understand how to connect the VS pins isolating from the VOUT.
Thanks for your response in advance....