Other Parts Discussed in Thread: BQ24210
1. Under the fixed installation of solar panels, does the VOC_CAMP connection method affect the MPPT regulation?
2. How does the bq25505 ensure that the battery is fully charged and does not damage the battery because there is no constant voltage and cross current charging mode of the battery management chip. Can you simply judge whether the battery is fully charged according to the VBAT_OV pin voltage?
3. What is the current that the MOS between VSTOR and VBAT can withstand? The maximum load of VSTRO in the circuit is 350mA. In the dark state, the battery needs to output 350mA current for about 10s.