Hello,
The datasheet has spec'd the SYNC pin upper threshold at two test conditions: VIN=PVIN=3V (2.45V) ~and~ VIN=PVIN=7V (4.25V).
We will have VIN=PVIN=5.8V. However, we don't know what the minimum VIH will be for the SYNC pin at this supply voltage. We would like to run it from 3.3V logic, but can't tell if this will be sufficient.
Also, some extra questions: What is the recommend maximum voltage on SYNC pin? (as opposed to the absolute max of 7.5V).
Can SYNC voltage exceed VIN/PVIN and go up to 7V regardless of supply? Or should it be limited to 5.8V in our case? (Bonus: if SYNC voltage shouldn't exceed VIN/PVIN, and VIN is not equal to PVIN, which one is the limiting factor: PVIN or VIN? I would guess VIN).
Thank you!
Regards,
Ryan B.