This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61241: VGS=VOUT

Part Number: TPS61241


Hi E2E,

I find current limit test conditions that is VOUT= VGS = 5V

Does the VGS mean PMOS of IC? But if VGS=5V, the PMOS can't work at all.

What is the VGS=VOUT=5.0V's meaning?

  • Hi Julian,

    I have to confirm it with our test engineer. 

    From my point of view, a current source is connect to L and Vout, high side mosfet is always conducted. Once current limit is triggered, one bit inside will be pulled high.