This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Help recommend buck-boost low power chips

Other Parts Discussed in Thread: TPS63031, TPS63802

Requirements are as follows:

1. Low power consumption. The quiescent current is as low as possible because it is battery powered;

2. Input voltage 2V~5.5V, output voltage 3.3V, output maximum current 0.35A;

3. I found the TPS63031 quiescent current is 25μA, I feel not low enough.