We recently tested a product utilizing the TPS63060 for a 5v buck-boost converter. We found that the product failed EMC in the range of 30MHz-100MHz with the largest peaks around 50MHz. The failure was noise coupled from the TPS63060 through to IO wires which left the board. What are the typical modes of noise coupling for the TPS63060 and are there any design suggestions to mitigate this? We were planning to put some 0.01uF caps on the input and output power rails, additional ferrites on the IO, and a common mode choke. Are these necessary or will any cause stability issues? Thanks