Tool/software: Code Composer Studio
Hello,
I'm using TPS65381A as companion power mangement IC for TMS570.
Problem is that operational amplifier around analog input of the TMS570 is powered by another 5V.
So, to protect analog input pin of TMS570,I should power off the 5V before TPS65381A shuts down.
But it is not easy. So, I am trying to place diode between 5V generated by TPS65381A and 5V.
But I worry if VDD5 pin is damaged or not in case 5V generated by TPS65381 shuts down earlier than 5V.
Please tell if VDD5 will be damaged or not by anther 5V.
Thanks in advance and best regard