Other Parts Discussed in Thread: LMR16006, LMR16010, LM5160
Hi team,
whether the LM5160A and LMR16006, LMR16010 can support the 5~53V input, 3.3v output? We want to check the Dmax. Thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Frank
You might be able to do it with LMR16010 but operating with a lower frequency such as 200kHz to avoid minimum on time.
for 5V input and 3.3V output your Dmax will be around 66% which is lower than 97% on this part.
For complete design you might want to check with webench
Thanks
-Arief
Yes it does not seem that webench can generate a design using this low input voltage with LM5160
Thanks
-Arief