Hi all,
I made a DCDC buck regulator, using the webench power designer, with LM5141RGER, I attach the design report. I use this DCDC converter with a voltage of 24V as VIN.
As you can see on efficiency graph, with a load of 2A and 24Vin, the efficiency should be about 95%. I tried on my PCB and with these condiction the efficiency is 83%.. Too low..
So I checked the part number of components, some signals, like HO, HOL, LO, LOL, but they seem all ok..
The heat dissipation is normal: only the mosfets and the inductance are more hot than the others components, and thy are at 32°C..
What can I check?
What can be the problems?
How can I do to improve the efficiency? I would like to reach the 95%..
WBDesign115 (1).pdfThank you in advance,
Have a nice day.
Diego.