Section 9.2.2.1 of the 2019 datasheet mentions using a series resistor on the CE/ pin to limit the current into CE/ during a negative voltage event. What is an acceptable current to allow, or what value resistor should I use?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Section 9.2.2.1 of the 2019 datasheet mentions using a series resistor on the CE/ pin to limit the current into CE/ during a negative voltage event. What is an acceptable current to allow, or what value resistor should I use?
Using the LM66100EVM, I can configure the board to the diode ORing configuration that I want to use ( see Figure 9 of datasheet).
If I connect Vin1 backwards (-3V), I get 282mA current flowing from Vin1 (with no load on Vout).
If I remove JP7 (1K resistor between GND pin of U2 and system GND), the current falls to 1.3mA. I am assuming the current is flowing from system GND, through the 1K resistor, into U2 GND pin, through the U2 CE/ pin and then out to the backwards Vin1 source.
Will -282mA hurt the CE/ or GND pin? Is -1.3mA an acceptable level?
Are there advantages to placing the series resistor in the GND circuit as opposed to the CE/ circuit?
Hi Steve,
I checked with the design team, -282mA shouldn't be an issue and won't damage the device. How long of a duration is the RPP event?
Thanks,
Arthur
Thank you for the information.
The RPP event could last several minutes before the end user realized the batteries were installed backwards. Therefore, I will add a series resistor to limit the CE/ current to a point where it does not overheat the LM66100 device.