Other Parts Discussed in Thread: CSD19534Q5A, CSD18540Q5B, , LM5176, PMP21278
I made a prototype as suggested by WEBENCH, using CSD19534Q5A and CSD18540Q5B and am currently working on a larger design incorporating the power supply. I have two questions related to the project:
1. The prototype appears to handle full design power (24V, 9A) at room temperature. To make sure that it can work at higher ambient temperatures (up to 60C), I am planning to parallel the FETs. Is it safe to assume that, everything else being equal, the gate drivers will handle the additional FETs just fine?
2. Is is ever recommended and/or allowed to use small (~10 ohm) gate resistors with LM5176-Q1?