This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS54331: Require 3.3V, 3A output with Minimum 3.5V input

Part Number: TPS54331


With the below given circuitry, can we able to get the Output 3.3V and 3A.

Please suggest at earliest. 

Thanks.