This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM3409HV: NOISE PROBLEM WITH INDUCTOR

Part Number: LM3409HV


Hello,

i designed a pcb based on AN-1953 LM3409HV evaluation board.

The max current is 2A at 40V for string led (10 leds).

I have 2 problem :

1) i heard "noise" on the inductor on my pcb when i put pwm signal on enable pin on the LM3409HV (same noise on evaluation board)...at 2 khz. If i change pwm frequency i have noise too at 3khz, 4khz etc...

i tried to change inductor with differents brands but it doesn't solve the problem.

2) when i use Iadj for analog dimming i can not turn off the light even putting 0V is it normal? i need to use enable pin for switch off the light?

Someone can help me please?