I have an issue when trying to use the TPS40200 to power a digital servo at 6V from an input voltage of 12V. The power supply works fine under resistive load conditions up to 1.65A but constantly reset from 0V to 6V when trying to power the servo. The current limit is set to 5A and the servo only uses 160mA. Is there some sort of impedance mismatch problem with using the TPS40200 to drive complex loads?
please help
thanks
Kyle