Hello,I would like to know how much current need when DCR010503 starts up without load,Thanks!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,I would like to know how much current need when DCR010503 starts up without load,Thanks!
Hi,
The DCR010503 input current needed at startup with no load is a typical of 18 mA.
Regards,
Alejandro
However, note that this device does not have a soft-start feature, which can cause an in-rush current of 1 A or greater depending on your input voltage ramp up.
Regards,
Alejandro