Other Parts Discussed in Thread: TPS61088
Hello team,
My customer is considering to use TPS61088-Q1 if the following can be meet.
Q1) When the system power up, the TPS61088 voltage is Vin= 0V and Vout = 12V created from other DC-DC converter. The period is maximum 10ms. The customer would like to confirm whether this situation causes the damage to TPS61088-Q1. Does TPS61088-Q1 have problem with this situation(Vin= 0V, Vout = 12V at TPS61088-Q1 pin)?
Q2) In some cases, TPS61088-Q1 Vin voltage may be larger than Vout voltage created from other DC-DC converter. Is it acceptable for TPS61088-Q1?
I think that It is special situation. Would you please advise?
Best Regards,
Akihisa Tamazaki