Hello All,
The datasheet of OMAP3503 processor is not having the clear information on the vdds_sdi, vdds_dsi, vdds_csi2 and vdds_csib power pins and how it should be connected to TPS65950. Can you please provide the following clarifications ASAP.
- Can we connect the vdds_csi2 (Dedicated power supply for CSI2 Complex I/O) to the VIO_1V8 (VIO DC-DC Regulator of TPS65950) as like in Beagle Board. Our camera subsystem interface requires 1.8V I/O. In SOM module and Mistral board, this is connected to VAUX4.
-
- What are the voltage and power specifications for the vdds_csi2
- What are the GPIO pins powered by vdds_csi2
- Is there any sequencing constraints applicable for this power
- Can we connect the vdds_csib (Dedicated power supply for CSIb Complex I/O) to the VIO_1V8 (VIO DC-DC Regulator of TPS65950). Our camera subsystem interface requires 1.8V I/O. In all the reference boards, vdds_csib is connected to VIO_1V8
-
- What are the voltage and power specifications for the vdds_csib
- What are the GPIO pins powered by vdds_csib
- Is there any sequencing constraints applicable for this power
- Can we connect the vdds_sdi (Dedicated power supply for SDI I/O cell) to the VIO_1V8 (VIO DC-DC Regulator of TPS65950). In all the three boards, vdds_sdi is connected to VPLL2. We are not using the Display Sub system and the pins are configured as GPIO inputs / outputs
-
- What are the voltage and power specifications for the vdds_sdi
- What are the GPIO pins powered by vdds_sdi. The datasheet specifies gpio_66 to gpio_93 vdds and not giving the vdds_sdi or vdds_dsi
- Is there any sequencing constraints applicable for this power
- Can we connect the vdds_dsi (1.8V analog power supply) to the VIO_1V8 (VIO DC-DC Regulator of TPS65950). In all the three boards, vdds_dsi is connected to VPLL2. We are not using the Display Sub system and the pins are configured as GPIO inputs / outputs
-
- What are the voltage and power specifications for the vdds_dsi
- What are the GPIO pins powered by vdds_sdi. The datasheet specifies gpio_66 to gpio_93 vdds and not giving the vdds_sdi or vdds_dsi
- Is there any sequencing constraints applicable for this power