This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61089: VOUT definition

Part Number: TPS61089

Hello Support team,

Could you please support below my question?

Q1. VOUT is defined as 12.6V@Max in TPS61089 datasheet p4. Recommended Operating Conditions.
Is this value at PWM mode?, In case of PFM mode, VOUT is increased 1% than PWM according to datasheet. Should we keep 12.6V at PFM mode?

Q2. VOUT is set by external resistance, R1 and R2. Even if we set both resistance to keep 12.6V, VOUT will be over 12.6V in case of maximum value of VREF as 12.236V.

Q3. Should we set R1 and R2 to keep VOUT less than 12.6V?
VOUT of Absolute Maximum is defined as 14.5V. Can we set Max of VOUT as 12.6~14.5V? What problem will be occurred at that condition?

Q4. If VOUT is less than VIN, what problem will be occurred?

Best Regards,
Hirokazu Takahashi