Hi TI
I want to find a Gauge. The specifications are as follows. Is there any recommendation?
Do you have this Pin to Pin with BQ27426?
1. Supporting capacity > 8000mAh
2. Supporting lithium ion and lithium polymer batteries
3. There is a non-volatile flash inside, and the configuration does not disappear when the power is turned off.
4, I2C Communication
5. SOC interrupt can be configured
6. Support configuration of Chem ID
7. It's better to be used on the system side
8. Impedance tracking method
Thank you
Jerry