Could you please share 1s battery charge efficiency data with our customer in 5VIN, 9VIN, 12VIN, respectively.
Would you also let us know if those are placed on Figure 4 to Fihure 7 of System Efficiency.
best regards,
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Could you please share 1s battery charge efficiency data with our customer in 5VIN, 9VIN, 12VIN, respectively.
Would you also let us know if those are placed on Figure 4 to Fihure 7 of System Efficiency.
best regards,
Hey Toshiro-san,
Please refer to Figures 4, 5, 6, and 7 in the datasheet for the system efficiency. Specifically, refer to the VOUT = 3.7V curves for the 1S configuration.
The data for charge efficiency can be directly derived from the system converter efficiency (in the figures above) by adding the I2R conduction loss of your customer's particular PMOS BATFET. Thus the efficiency of the charger is the system efficiency @ charging current minus I2R loss at charging current due to the external BATFET RDSON.
As an example, with 5VIN, 3.7VOUT, 1A Output Current, System Efficiency is ~92%. Let's assume the charging current is 1A, and the BATFET RDSON is 20mOhm.
The new efficiency can be calculated by the following:
(1/eff_new) = (1/eff_prev + Ploss_new/Pout).
In our example, the new loss = ICHG^2 x Rdson = 0.02W. New efficiency = 91.54%.
Regards,
Joel H