I read an answer to one of the customers question regarding time EN and Vout ,the delay between EN and Vout at Il=0.25A,V out= 5.0v is approximately 5ms. i am using LMZM23600 as a replacement design to an existing design. LMZM23600 is quite apt for me because of its small size with given i/p and o/p specs. because of 5ms delay built in test is failing. is there any way i can reduce this delay? All i/p and o/p caps as suggested. linear regulator is hogging current because of low efficiency. pls advice.
regards