This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCD90120A: Current Measurements in TI Fusion

Part Number: UCD90120A

Hello,

I have configured the UCD90120a to calculate current, however, the values I'm getting are extraneous.

The equation looks something like this:

V=64.194mOhms(I)+1.17V

I have input 64.194 mOhms for the Igain and -15 A for the Ioffset. However, when I read the current it gives me an absurd value. I was wondering how this number is calculated since I have not seen an actual calculation for the current.

thank you,

Jordan