Hi Team
I'd like to be advised about proper LED driver which can support below my requirement.
I found TLC59116 is closer but is not best.
Would you advise TLC59116 is the best suggestion?
Requirement
1. Number of LED CH: 32 required
2. Current per CH: Max 200 mA
The number of simultaneously lit CH at maximum current is 2 CH
For 2 CH or more, Max 400 mA or less limit
3. Tr / Tf: about 1 us
4. I want to monitor the current value of each CH
5. Current limit, temperature shutdown function
6. Current value adjustment function (5mA step)
Thanks
Best regards,
Shidara