This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61178: Lower BST Capacitor Value

Part Number: TPS61178

Hi,

FYi, my application of this IC is Vin=5V(usb), Vout2=13V. The Vout2 is then, supplied to Audio Amplifier.

From the TPS61178 datasheet, the BST capacitor value was recommended at 0.1uF ~ 1uF. 

What if the design is using a lower value, for example 0.047uF? What is the side effect such as the performance, reliability, etc?

Thanks,