Other Parts Discussed in Thread: BQ25883
Hi
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Jeff-san
Yokota-san,
The voltage regulation accuracy is not directly related to the point of regulation. For the BQ25883, the point of regulation is between the IC's BAT and GND pins. You can force the BQ25882 to regulate at the BAT and GND pins by connecting BATP and BATN to those pins at the IC. For the BQ25882 with VBATREG=8.4V, the regulation accuracy is 8.3664V to 8.4336V over -40C to 85C. For the BQ25883 with VBATREG=8.4V, the regulation accuracy is 8.35V to 8.44V over 0 C to 85C.
Regards,
Jeff