This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS62130A: Light load efficiency 1.5uH, 2.2uH

Part Number: TPS62130A


Hello Support team

 

I simulated the efficiency of TPS62130A at both of 1.5uH/10.7mΩ and L=2.2uH/19mΩ with Webench.

 TPS62130 effeciency(2019 06 24).pptx

2.2uH model

https://webench.ti.com/appinfo/webench/scripts/SDP.cgi?ID=63A426F9A7F4FE3C

1.5uH model

https://webench.ti.com/appinfo/webench/scripts/SDP.cgi?ID=72C36E2DCB7F6CE6

 

The efficiency at 1.5uH is better than one at 2.2uH as the chars of webench.

Could you let me know why 1.5uH case is better performance than 2.2uH case at 0.001A (PFM mode)?

 

2.2uH : 81.2%

1.5uH :84.3%

 

Best Regards,

Hirokazu Takahashi