This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24610: BQ24610

Part Number: BQ24610

Hi,

We are planning to use BQ24610 for our battery charging circuit.

In reference design you have use 35V rated capacitors from PACK+ to GND

In our design we are using 8.4V battery.

Can we use 16V rated capacitors for this. 

Regards,

Shafeeq

  • Shafeeq,

    Yes.  We use higher rated cermaic capacitors to account for the derating that occurs when ceramic capacitors have a voltage applied.  The general rule is to use capacitors with 2X their expected maximum applied voltage. The capacitor manufacturer can provide a derating curve.  I also suggest using X5R or better capacitors.

    Regards,

    Jeff