I understand that I can query the UCD9090A's internal temperature sensor using the READ_TEMPERATURE_1 PMBus command. However, I cannot find any documentation that provides that sensor's technical capabilities.
Can someone please provide the temperature range that the internal temperature sensor is able to report? I don't want to assume that it is the UCD9090A's full operating range of -40C to 125C, but it is likely at least that. Second, can you also please provide that internal temperature sensor's accuracy? In other words, what is the tolerance on the reported temperature?
Thank you,
Jim