HI
We are planning to develop PSE module related to POE and want 8ch configuration with 40W power for each channel.
If you look at the datasheet, you should apply 2Pair to all, and it seems that 40W class design is possible, and I think you have to use two TPS23880 to construct 8Ch. Is this my idea?
Or, you can use a single TPS23880 to make sure that you can design 40 watts for each 8ch.
If you have additional 40W schematic for your design and applicable FET, please share.
Also check if the output voltage can be designed as negative.