Other Parts Discussed in Thread: TPS24740
Hi,
I have questions below. Here's my condition:
TPS24712 will applied at PCIE card hot-plug.
Vin=12V, Cout=3000uf, MOS=NTMFS4H01NT1G
iLOAD=
1. 18.3A (200uS)
2. 14.2A (1mS)
3. 12A (5mS)
4. 5.5A (TDC)
1. The max peak current is 18.3A(200US), can i set Rshunt=1.5mohm to got OCP=16.7A? And set timer longer than 200us to make sure gate won't pull down?
2. PG will be low immediately when load hit current limit point? Or need to wait timer expired?
3. Only current will trigger timer count?
4. Do i need to use back to back MOSFET? If the load board will be removed and plug back immediately(load board has large cap and still hold 12V), will the reverse current through body diode back to VIN?
Jack CT