This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ35100: Query on measuring 200uA using accumulator mode

Part Number: BQ35100


Hi,

I want to use BQ35100 for Li-SOCl2 Primary battery of 19Ah for its remaining capacity measurement during operation. Continuous load on the battery is 200uA and hourly once load current goes to 30mA(average) for a duration of 500ms. As currently my product do not know state of battery charge capacity so I want to introduce BQ35100 to know the % of battery capacity remaining. Do you recommend me to use BQ35100 to use for the above requirement?

Secondly if I can use BQ35100 for the above application then from my understanding on the IC I have selected to use Accumulator mode for measurement of charge remaining capacity of the battery.

I have question that if through I2C micro sends command to start the operation for battery health monitor and stop command after 5days to know the battery state of health then can I know the state at the end of 5day.

 

Thanks,

Rahul Wagh