Other Parts Discussed in Thread: BQ78350, , BQ78350-R1, BQ34Z100, BQ76930, BQ76940, BQ34110, BQ34Z100-G1
Hello;
I note that the bq78350 includes its own AFE, ADC and Coulomb Counter, but when used as a companion to the bq76920, it seems these are not used(?). Rather, its datasheet says "The bq78350-R1 device continuously monitors the measured current and integrates the digital signal from the AFE (the bq769x) over time, using an internal counter."
In contrast, the bq34z100's datasheet shows its "companion" controller (the NRD bq77908) also attached to the sense resistor. ??
I need the scalability featured in both gauges, but not on the 76920, and so it would seem I would need to have the gauge do the measuring.
Please clarify. Thanks