I have an application switching 5V to a high impedance signal. When the switch is off the impedance to ground needs to be very high (greater than few 100K).
The TPS22810 states there is no discharge resistance when the QOD pin is left floating but I am seeing about 50K to ground, which is too high for my application.
It it expected to see about 50K to ground even when the switch is off and the QOD pin is floating?
If so, can you recommend any other load switch for ~5V at 600mA, higher than 300L with an output slew rate of less than 2mS?
BR,
Steve