This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM3559: Turning On Torch Without TX1/TORCH/GPIO1 Pin

Part Number: LM3559

I want to turn on the torch mode of the LM3559 purely through register writes, and not using the TX1 pin.  It's not clear to me from the datasheet that this is possible.  What register configuration would do this?

Enable (0x10): 1a (Torch mode)

Torch Brightness (0xa0): 0x09 (56mA)

What else is required?

Thanks,

Chris