Other Parts Discussed in Thread: BQ34Z100
Im wondering whether I can use bq34z100-g1to monitor a substring of 200V lead acid battery which has 6V cells without actually putting any resistor in series with the cells.
My goal is to measure health of the cell(s) by connecting the sense resistor in paralell to the measured cell (lets say one 6V cell) for a moment and then measure the internal resistaance/impedance of the cell with help of bq34z100-g1, then disconnecting the resistor from the cell again (using sir, relay or mosfet or something)
Is this simething I can use the bq34z100-g1 for? My goal really is to provide a one off measurement of the health of sections of the battery pack without the requirement to disconnect the cells to add sense resistors.