Hi team,
I would like to know the maximum VOL of TPS3851G33EQDRBRQ1 at VDD=3.3V.
VOL maximum is specified at VDD=5.0V and Ireset=3mA and is 0.4V.
Since the VIL max of the target IC's reset pin is 0.35V, I would like to know if this is feasible to control using this device at VDD=3.3V.
It is nice if you can share VDD=3.3V version of Figure13 and Figure14 in the datasheet.
regards,