This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Asking for the recommendation on the charger solution

Other Parts Discussed in Thread: BQ25606, BQ25601D

Hi Team,

Customer is looking for recommendation on the charger solution.

Would you please recommend the proper solution for charger?

 

Below is the high-level requirement for the charger IC.

 

1. Support Li-Poly battery with 1500-2000mAhr capacity, 3.7V nominal, 4.2V Charging Cut-off. 

2. 1500mA above charging current (BC 1.2, or PD.)

3. Main chip (uC) USB interface available 

System Block diagram

https://txn.box.com/s/7wrlxl990w7p6sojkddpsahnnabqip8j

 

Thanks for help. 

BR,

SHH