This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ40Z60: Can't get a valid charge termination

Part Number: BQ40Z60

Hi all,

Following datasheet , the condition for a valid charge termination are :

All of the following conditions must occur for two consecutive 40-s periods:
Charging (that is, BatteryStatus[DSG] = 0) AND AverageCurrent() < Charge Term Taper Current AND Max cell voltage1..4 + Charge Term Voltage ≥ ChargingVoltage() / number of cells in series AND The accumulated change in capacity > 0.25 mAh.

In our case, we cannot reach Valid termination because the condition : Charging (that is, BatteryStatus[DSG] = 0)  does not have a duration of more than 10 sec

What condition can make BatteryStatus[DSG] = 1 after a complete charge of the battery ? 

Regards

Gilles