This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ28Z610EVM-532: Configure for a single cell

Part Number: BQ28Z610EVM-532
Other Parts Discussed in Thread: BQSTUDIO, EV2400, BQ24105

Hello,

Apart from shorting 2p-1p terminals on the battery side to support a 1-cell operation, is there any changes to be made in the BQstudio to support this?.

when i connect a battery pack the bqstudio shows 0% @ 3.6V.

Also, when i press the switch S1, the gauge is momentarily connected to the EV2400 but soon after disconnects. chg fet drive is at 1.8V (1/2 of cell voltage) and dsg fet is at 0v.

there is no power supply or load connected to the pack terminals.

dont know what i am doing wrong......

Thank you,

Gaurav