This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ51021: Developing with BQ24160

Part Number: BQ51021
Other Parts Discussed in Thread: BQ51013, , BQ24160, BQ500212A

We are developing a system with BQ24160 and BQ51021.  We have USB going into the BQ24160 USB Input, and we have the output of the BQ51021 going to the VIN input of the 24160.  Our wireless charging is only meant to trickle charge our system.  We charge our 1400mah battery at 1A when using USB, but set the current limit of wireless charging to only 350mA.  We just migrated our design from the BQ51013BRHLT to the BQ51021 so we could use the I2C interface to send data to our wireless charger.  The system was stable using the BQ51013.  We are getting the system up and running right now, but we are seeing the wireless charging connecting, the current goes to the limit then it decreases down to a low current in steps and then after a few seconds it re initiates back to the higher current and repeats.  We don't want the current to constantly be ramping back to max current.  Is there some i2c settings I should be looking at to better setup the device?  The battery in this case is close to full, so it should just go to a low current output, equivalent to no load.