This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ27426: BQ27426-G1

Part Number: BQ27426

AtRate() mA
UnfilteredSOC() %
Temperature() 0.1K
Voltage() mV
Flags() nil
NomAvailableCapacity() mAh
FullAvailableCapacity() mAh
RemainingCapacity() mAh
FullChargeCapacity() mAh
AverageCurrent() mA
TimeToEmpty() min
FullChargeCapacityFiltered() mAh
SafetyStatus() nil
FullChargeCapacityUnfiltered() mAh
Imax() mA
RemainingCapacityUnfiltered() mAh
RemainingCapacityFiltered() mAh
BTPSOC1Set() mAh
BTPSOC1Clear() mAh
InternalTemperature() 0.1K
CycleCount() counts 0 65535
StateofCharge() %
StateofHealth() %/num
ChargingVoltage() mV 4000 4600
ChargingCurrent) mA
PassedCharge()
DOD0()
SelfDischargeCurrent()

what is the minimum and maximum range of these parameters ?