This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5170-Q1: LM5170 dual-channel current is different at low temperature

Part Number: LM5170-Q1
Other Parts Discussed in Thread: LM5170

    LM5170-Q1 dual-channel output current is not equal at low temperature -20°~-40°, one channel current is 44A, the others is 40A, but I set the same current by software. The two channels are the same current or too much difference in normal. The data as below:

standard 

44A -ISET(Iout1)

44A -ISET(Iout2)

25

44.56445313

43.67578125

-20

44.29785156

42.52050781 

-37

45.54199219

40.4765625

-37

44.7421875

40.4765625

-35

44.65332031

40.74316406

-37

44.38671875

40.83203125