Part Number: TPS25921L
Other Parts Discussed in Thread: LM66100
Hello,
My application needs all the standard circuit protection and I plan to use TPS25921L eFuse part right at the 5V power inlet into the system. Typical operating voltage and current conditions are 5V and 400mA. There is a large 2200uF (or higher) capacitor load after eFuse for which charging current will be limited to around 600mA. I have not performed all the calculations for TPS25921L yet to check if this can be achieved. There are a couple of 3.3V/3.5V LDOs further downstream. The large cap is needed to prevent interruption of a write in the MCU with integrated flash in case of power loss.
The application also needs reverse polarity protection on the input and reverse current protection from the large 2200uF cap. To keep cost low, I plan to use a low-drop Schottky diode on the eFuse input for reverse polarity protection. My application does not allow me to put the Schottky diode on the Ground path.
Question is whether the Schottky diode on the input of eFuse also provides reverse current protection from the cap and if the TPS25921L part is safe to use in this configuration.
I'd appreciate your thoughts and any potential gotchas or issues to keep in mind.
Thanks,
Satish