This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Buck-Boost/Boost Converter

Other Parts Discussed in Thread: TPS63802

Hello,

I am looking for a Buck-Boost / Boost Converter for my GPS based Tracking Application.

Tracker Device 1 Requirement

Vin: 1.2V ~ 3V

Vout: 3.3V

Iout: 300mA~400mA  [my Device Consumption is 250mA]

IQ: I need the lowest one

Tracker Device 2 Requirement

Vin: 1.8V ~ 3.6V

Vout: 3.3V

Iout: 300mA~400mA  [my Device Consumption is 250mA]

IQ: I need the lowest one

Kindly suggest me the suitable nano Power Buck-Boot / Boost Converter device.

Thanks,
Rahul